AXIS#.PL.INTINMAX

Description

AXIS#.PL.INTINMAX limits the input of the position loop integrator by setting the input saturation.  When used in concert with AXIS#.PL.INSATOUT, this variable allows you to make the position loop integrator effective near the target position. Far from the target position, however,the integrator is not dominant in the loop dynamics.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

N/A

Data Type

Float

See Also

AXIS#.PL.FB

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Related Topics

AXIS#.PL.ERR | AXIS#.PL.ERRFTHRESH | | AXIS#.PL.ERRWTHRESH | Position Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen